AnsweredAssumed Answered

Linux Device Driver for ADV7403

Question asked by shravan on May 4, 2012
Latest reply on May 9, 2012 by mhennerich

Hi all,

           Im having a custom made board of ADV7403. I have to write the linux device driver for ADV7403. Im a new to linux device drivers and i dont know where to start. From other posts i came to know that there is no linux device driver for adv7403. In this scenario linux device driver of which IC can be adopted so that i can modify these drivers to work for adv7403. If this is not possible how do i start writing the linux drivers for adv7403 from scratch.?

 

I have checked the working of adv7403 by using a micro controller and im able to communicate to adv7403 via i2c protocol.

 

Note: il be integrating this adv7403 with beagleboard which has DM3730 processor and linux kernel 2.6.32 ported on to it.

 

My system configuration: Intel Core 2 duo 2.93GHz, 2GB RAM

OS: Ubuntu 10.04 (kernel : 2.6.39)

 

If i have missed out any information that is required, please point it out.

 

thanking you,

Shravan Kulkarni

Outcomes