AnsweredAssumed Answered

questions about pipeline viewer

Question asked by lzping on Apr 28, 2012
Latest reply on May 7, 2012 by CraigG

in the picture,the number one point to  the first instruction in the program.

Why does the number 2 refers to the number of cycles is 624 instead of 1 in the picture.

Why does  the number 3 point  'j0=0x40000'  is repeated 6 times  in the picture.

Why does  the number 3 point  'j0=0x40000' of PD and  'j0=0x40000'  of  F4 in the same cycle, rather than delay of one cycle  in the picture.

Attachments

Outcomes