AnsweredAssumed Answered

No audio data on the output of processor AD1953

Question asked by Radim on Apr 28, 2012
Latest reply on May 20, 2012 by Radim

Hello,

I'm working on a project of a digital equalizer with processor AD1953. I designed my own hardware and tried to resuscitate the equipment, but there is no audio data on the outputs of AD1953, just a DC component. To be more specific a voltage 0,9 V occurs on pins VOUTL-, VOUTL+, VOUTR-, VOUTR+ and voltage 1,0 V on pins VOUTS-, VOUTS+. I measured clock rates on the corresponding pins and they seem to be right. On the MCLK0 pin there is a frequency about 12,24 MHz (256 * fS), on the BCLK pin 3,08 MHz (64 * fS) and on pin LRCLK there is frequency about 48,0 kHz (fS). Sample rate of audio is 48,0 kHz. Where could be a problem, if there is not any audio on the output?

Thank You for Your answer.

Outcomes