AnsweredAssumed Answered

ADF5350 - Will Phase Resync work with divided output?

Question asked by ELADI on Apr 26, 2012
Latest reply on Apr 30, 2012 by icollins

ADF4350 - Will the divided frequency outputs (anything below 2200 MHz) also work with the phase resync feature. From the block diagram, it appears that both the fundamental and the divided frequencies are fed to a multiplexer, and that multiplexer feeds the phase detector, so it is not clear to me what is actually being fed back to the phase detector.



Outcomes