AnsweredAssumed Answered

ADDS-BF535-EZKITLITE compatability with VisualDSP++ 5.0 Update 10

Question asked by superdupercooper on Apr 25, 2012
Latest reply on Apr 27, 2012 by superdupercooper

Hi

 

I recently acquired an ADDS-BF535-EZKITLITE to have a play with.

 

When I first turned it on it was running a basic 'flash the LEDs' program, but I have been unable to successfully upload anything to it.

 

I started with VisualDSP++ 3.5, and then upgraded it to v5.0 upgrade 10 (IIRC), but still no joy.

 

I've seen an announcement somewhere which says the BF535 was made obsolete when AD reworked their eval boards to be RoHS compliant, but surely I should have got some joy out of v3.5?

 

It's installed on Windows XP SP3.

 

Any ideas or am I flogging a dead horse?

 

Cheers

 

also, i'm getting identical behaviour on two different PCs.

Outcomes