AnsweredAssumed Answered

Re: Need Help with ADSP 21369 for Audio Processing - using SRAM/SDRAM in simulator

Question asked by grossi on Apr 23, 2012
Latest reply on Apr 30, 2012 by CraigG
Branched from an earlier discussion

@ Home i use only the Simulator but in the Lab at the University i can work with a EZ Kit.

 

It works so far=)  but my Problem is to get bigger Files in the Simulator (over 100 KB), so i will try my programm with bigger Audiofiles and Impulseresponses without any Board.

 

Is it possible to use the SRAM or SDRAM in the Simulator ? Because PMDA and DMDA are to smal for my input files.

Outcomes