AnsweredAssumed Answered

ADuCRF101

Question asked by BenjaminHo on Apr 20, 2012
Latest reply on Apr 25, 2012 by AudeR

1. for ADuCRF101, the frequency bands, 862 MHz to 928 MHz and 431 MHz to 464 MHz, so for 862MHz to 928MHz, how do I configure RF frequency to 868MHz or 915MHz, software or hardware configuration? where can find more detail info

2. For PA , there are Single end & differential PA internal, beside output power different, what is the factor to choose single end or differential PA?

3. in UG-231 (ADuCRF101 User Guide) - I confuse on Figure 33: Combined Single-Ended PA and LNA match & Figure 34: Separate Single-Ended PA and LNA Match, the connection is the same, so what the different?

Outcomes