AnsweredAssumed Answered

BF506F Booting from UART

Question asked by G.Bit on Apr 19, 2012

Hello,

in my project it is necessary the boot from UART, I connected UART0_RX, UART0_TX and UART0_RTS at the host(through an MAX3232). I built my code as loader file, UART Boot Mode, Binary Boot Format and 8-bit Output Width but it didn't work.

Could you tell me what the VisualDSP++ project options is necessary to create a loadable .ldr file bootable through UART? Could you show me same example?

Thanks in advance.

G.Bit

Outcomes