rbrennan

ADF4193, ADF4196 evaluation boards software

Discussion created by rbrennan Employee on Apr 11, 2012
Latest reply on Jul 3, 2012 by rbrennan

The latest ADF4193 and ADF4196 software (v6) is attached.

 

Installation process:

1. Disconnect any evaluation board

2. Download and run the attached installer

3. Click Next/Continue/Finish when asked

4. Connect your evaluation board

5. Windows will detect the evaluation board and install the drivers

6. Run the ADF4193-6 software from the desktop or Start Menu

7. The status bar of the software should show that the board is connected. If not, try disconnecting and reconnecting the board.

 

Installer includes USB drivers.

 

Reply to this thread if there are any issues.

 

v6.3: reduced window size; improved initialization sequence.

v6.2.1: added warning if MOD < 13

Outcomes