AnsweredAssumed Answered

Two input voltages (5v and 24v), but only single output voltage needed

Question asked by cklooi on Apr 11, 2012
Latest reply on Apr 23, 2012 by LucaV

I need to make following IC circuit which can have the function to switch between two input voltages

 

 

1. Input voltages = 5V and 24V

2. Single Output voltage = either 5V or 24V (as only one voltage will be used at a time)

3. If possible, function to turn off both is welcomed too.

 

 

Does ADI have solution for this scenario?

Outcomes