AnsweredAssumed Answered

ADV7179 giving mono output

Question asked by HankZ on Apr 6, 2012
Latest reply on Apr 11, 2012 by Ray.Thomas

Hello,

 

We are using the ADV 7179 in NTSC square pixel mode, with a 24.5454 MHz clock. The output is displayed only in black and white, even when using the internal color bar test pattern.

 

We are in mode 0 slave option, using DAC A CVBS output, and our register programming is as follows:

 

MR0: 0x00

MR1: 0x38

MR2: 0x01

MR3: 0x00

MR4: 0x10

TR0: 0x08

TR1: 0x00

FSC3: 0x55

FSC2: 0x55

FSC1: 0x55

FSC0: 0x25

 

Do you see a problem with the configuration? Is there something else that could be causing this problem? Any help will be greatly appreciated.

 

Thank you,

Outcomes