AnsweredAssumed Answered

adv 7842 hdmi graphics

Question asked by pgQuest on Apr 5, 2012
Latest reply on Apr 5, 2012 by GuenterL

Hello

 

Table-3 reports that the maximum resolution supported for HDMI-GR mode is 1280x1024@75.  Can i still feed 1080p@60 DVI - RGB input to the chip? If yes then can i still use the HDMI-GR mode? (Can i modify and use the script ":5-8c 1920x1080@60 RGB in_ 444 24bit H_V_DE DVI" which is configured in  autographics GR mode )

 

Regards

PG

Outcomes