AnsweredAssumed Answered

AD9517 reference I/P and Clock I/P

Question asked by Vishnu on Apr 4, 2012
Latest reply on Apr 4, 2012 by pkern

Hi,

 

When the internal PLL of AD9517 is used, I need to use the REF pins and in clock distribution mode, I should use CLK pins. Is it possible to tie both these pins together with a capacitor (so that the common mode bias doesnt get affected)?

If I can do like that, then I will be able to switch between both these modes, without change in hardware. Only a software change is required.

 

Regards,

Vishnu

Outcomes