AnsweredAssumed Answered

AD5932 working with slow Mclk?

Question asked by DanTech on Mar 27, 2012
Latest reply on Apr 17, 2012 by DanTech

Hi,

 

I just got an AD5932 and its evaluation board. Im looking for a frecuency generator suitable for my project which needs frequencies between 40kHz and 100 kHz with sweeps around 0.01Hz between 2 consecutive steps. According the maths in the datasheet that would be possible with a slow external clock but I can try it because the evaluation software only supports MHz frequencies. So, my question would be, it is possible to use this device with a Mclk of 90kHz or similar?

 

I know that I could try it with a microcontroller but I dont have any and I would rather know if it is possible before buying anything else. I just need to know if it will be possible.

 

Thanks in advance

Outcomes