AnsweredAssumed Answered

ADAU1701 I2S Input

Question asked by DefTech on Mar 21, 2012
Latest reply on Jun 5, 2012 by DefTech

Hi,

 

I have a working ADAU1701 solution using Analog Inputs but need to add an external SPDIF with SRC @ 48k output to the design.

Setup as follows and attached jpegs:

 

1) ADAU1701 as Slave to external 256fs MCLK.

2) Data, BITCLK, and LRCLK connected to MP1-Input Sdata-1, MP4-Input LRCLK, MP5-Input BCLK and MCLKI

3) SCH Input Block 1,2,4 & 5 Active 

4) Programable MUX Nx2-1

 

 

Note: when using Analog input and SPDIF Not Locked signal throughput is good.

 

Note: when SPDIF locks and all data and clks present at ADAU1701,  MUX switched to I2S input 4&5, result is NO signal throughput.

 

What am I missing???

 

Are there any eval applications available with I2S functioning?

 

What is the 1701 expecting for BIT Clk rate 64fs?

 

Is I2S 24Bit input OK?

 

Thanks,

Daniel

Attachments

Outcomes