AnsweredAssumed Answered

CONFIG_SILENT_CONSOLE still doesn't work with spi flash (2011-RC5)

Question asked by illishar on Mar 20, 2012
Latest reply on Feb 7, 2014 by Aaronwu

I've just downloaded the u-boot 2011-RC5 and is using the bf518f-ezbrd configuration.

 

I'm a little disappointed to find out that the CONFIG_SILENT_CONSOLE still isn't working when using spi flash. Yes, it works if you predefine the "silent" in your env. But removing it from env or adding it won't work. It's due to the "relocating of the env" sequence.

 

The CONFIG_SILENT_CONSOLE is widely used. It would be really nice if it also worked.

Outcomes