AnsweredAssumed Answered

AD1974 Daisy Chain

Question asked by dlh on Mar 19, 2012
Latest reply on Jul 2, 2013 by joserra000

Hi,

 

1) Regarding the AD1974, the data sheet mentions that 16 channels are supported. However, the example of daisy chaining the AD1974 only shows two addition devices - is it in fact possible to connect 4 x AD1974 together?

2) If 4 devices are supported, how are they connected, are there any example schematics etc?

3) Can a single 12.288mhz oscillator drive all the clocks directly and support 48khz sampling rate for all 12-16 channels?

4) Finally, the data sheet shows the connection with a Sharc with ABCLK going to both TxCLK and RxCLK. Why is does it need to go to TxCLK?

 

 

Thanks

Outcomes