AnsweredAssumed Answered

The specifications of the cable inputted into ADV7612

Question asked by avjkf on Mar 13, 2012
Latest reply on Mar 13, 2012 by DaveD

Hi,

My customer is using ADV7612 in their prototype.

They want to input up to 2.25Gbps signals and whose lengths of cables are up to 30meters .

The ADV7612 Datasheet rev.C describes

'It is capable of equalizing for cable lengths up to 30 meters to achieve robust receiver performance.'

My customer wants to know if there are any recommendations about the specification of cables.

For example, ADV7612 can equalize more than xx meters of xx AWG cable at 2.25 Gbps. etc. as AD8195 datasheet describes.

If there are, could you please tell me?

Thanks.

Outcomes