AnsweredAssumed Answered

Porting BF533 restore from hibernate to BF52X

Question asked by G40 on Mar 7, 2012
Latest reply on Mar 8, 2012 by CraigG

Following on from http://ez.analog.com/message/44624#44624

 

I am trying to get this code to run on the BF526 EZ board. My hi-tech approach has been to change the machine specific include files and target processor. All compiles/links except for the init_code where I get this failure:

 

----------------Configuration: Init_code - Debug----------------

Linking...

 

[Error el2011]  Invalid memory range and/or width for memory 'PROGRAM'

 

Linker finished with 1 error

cc3089: fatal error: Link failed

 

The BF533 init code LDF file defines PROGRAM like this:

 

//    PROGRAM   { TYPE(RAM) START(0xEF000000) END(0xEF0003FF) WIDTH(8) } //Boot Rom
    PROGRAM   { TYPE(RAM) START(0xFFA09000) END(0xFFA13FFF) WIDTH(8) } //L2
    SDRAM   { TYPE(RAM) START(0x00000000) END(0x07FFFFFF) WIDTH(8) } //SDRAM
//    PROGRAM   { TYPE(RAM) START(0x20000000) END(0x23FFFFFF) WIDTH(8) } //ASYNC BANK 0
//    L1_CODE   { TYPE(RAM) START(0xFFA00000) END(0xFFA03FFF) WIDTH(8) } //

 

What is the equivalent for the BF526? Any init code examples for this family would be very helpful.

 

Many thanks

 

Jerry

Outcomes