AnsweredAssumed Answered

Digital audio connection ADAU1701

Question asked by rastariot on Feb 29, 2012
Latest reply on Mar 5, 2012 by rastariot

Hi all,

 

struggling over the digital connection for connect two ADAU1701 devices (again...).

 

In my setting the Master delivers all clocks and routes (MP10, M11) back to its own clock inputs (MP4, MP5) and to the slave DSP inputs (MP4 and MP5). I can deliver audio from master to slave but cannot see any audio date coming out from the slave!

 

Here´s my question: Must I also connect the clock signals from the master to the clock outs from slave(MP10,MP11) for some reason?

 

Or do I have to select both as masters for the clock output?? I am confused

 

Any help is welcome1

 

with best regards,

rastariot

Outcomes