AnsweredAssumed Answered

Running I2CWSD.exe as a command line for ADuC7023

Question asked by ArnaudLEM on Feb 29, 2012
Latest reply on Sep 20, 2012 by EckartH

Hello,

I need to automatically download a firmware into an ADuC7023 through the USB-I2C/LIN-CONV-Z dongle. To do so I want to run the I2CWSD.exe program as a command line. Formerly we used a program called ARMWSD.exe to do the same thing with the ADuC7024, the command line looked like that: ARMWSD.exe af=path_to_firmware aa=y ap=ADuC7024 fe=n ......

Does anyone knows if this is also possible with I2CWSD.exe and if so could you direct me to a documentation describing the available arguments.

Thanks for your help.

Outcomes