AnsweredAssumed Answered

Is it possible to use the EVAL-5680 with LabVIEW

Question asked by amills on Feb 22, 2012
Latest reply on Feb 23, 2012 by amills

Hello,

I have purchased an evaluation board for the AD5680, a Single Channel, 18-Bit, Serial Input, Voltage Output DAC.  I would like to use this in a single application, and therefore it would be helpful to simply use the evaluation board.   AD provides a GUI based program which converts the hex word into a command and the unit outputs a voltage proportional to that hex word.  

 

National Instruments has a wizard that can be used to produce a driver for a USB device, provided one has a list of commands, the USB vendor ID number and the product ID number.

 

Are these available?  Alternatively, is there a way to communicate with the eval board?

 

Thanks,

Outcomes