AnsweredAssumed Answered

Power AD7685 - Multiple Supplies - Power Sequence

Question asked by CRFA on Feb 21, 2012
Latest reply on Mar 15, 2012 by CRFA

Hi,

 

I would like to know if there's a recommended practice for power-up the different supplies of the AD7685. I'm designing a battery operated device which has the following sections: Sensor, Signal Conditioning Circuitry, AD7685 and MCU.

 

I have three supplies:

- Vref. 3.0 V. Connected to Sensor and Vref pin on AD7685.

- 3.3V Analog. Connected to VDD on AD7685 and to supply the signal conditioning circuitry (op amps, filters,...).

- 3.3V Digital. Always On. Connected to VIO on the AD7685 and the rest of digital circuitry, including MCU.

 

What I would like to do, is the possibility to turn OFF/ON the Analogue section (Vref and 3.3 V Analog) while leaving always ON the digital circuitry.

 

It's okay to leave the VIO power ON and cutting the supply to VDD and Vref ? Or should I connect VIO to VDD (then becoming part of the 3.3V Analog supply)?

 

The lines: SDI, SCK, SDO and CNV are connected to pull-up resistors to the 3.3V Digital Supply and to a MCU.

 

Regards,

Attachments

Outcomes