AnsweredAssumed Answered

Amplitude ramp between two non-zero given levels (AD995x)

Question asked by Rice on Feb 20, 2012
Latest reply on Feb 21, 2012 by DSB

Hallo,

 

I need to perform amplitude ramps between two non-zero given levels (eg. from 0x12DF to 0x38D7 values of amplitude digital word and vice-versa). I have been working with the AD995x DDS family but it seems impossible to do.

 

With the OSK pin I can perform ramps between zero and a given level... and using the RAM registers I can only perform ramps between two (or more) levels in case of phase and frequency.

 

I am missing something or is that just impossible to do? If it is so, can anybody tell if any DDS which can perform this kind of ramps?

 

Thank you very much.

Outcomes