AnsweredAssumed Answered

adsp 21479 parallel flash programming

Question asked by bansal on Feb 17, 2012
Latest reply on Mar 1, 2012 by CraigG

sir in my borad i m using adsp 21479 sharc processor  . i designed my board similar  to 21479 EZ kit. when i m trying to load driver for flash parallel programming,it is showing 0.2 silicon problem,

 

i have used 25 MHz instead of 16.625 MHz, and CFG pin i m using '00' configuration for multiplication of 8 time frequency, and all other things are same as EZ kit.i m using parallel flash memory M29W320EB. when i load flash programmer driver it shows error,

 

is there any i have to change in the code of EZ21479parallel_flash drive.dxe (214xx/example/flash_programmer/parallel) ? and where i have to change in the program ?

or is there any other solutions ?

Outcomes