AnsweredAssumed Answered

Aduc7061 ADC reference

Question asked by abcdoaabc on Feb 17, 2012
Latest reply on Feb 21, 2012 by MMA


Hello.

ADuc7061 ADC reference source can be determined by the sensor power resistor divider get? ( 50ppm resistance 0.5%), composition ratio mode, reduce the power fluctuations due to the influence of.The aduc7061 ADC application, in order to reduce the power consumption, the main ADC multiplexed pins, configuration of ADC0 / ADC1 ( differential mode ) pressure collection PGA set amplification was 256, ADC2 / ADC3 ( differential mode ) temperature collection PGA set amplification of 1. This way has a problem?

Outcomes