BrettG

[Bug Report] Flangers do not save settings

Discussion created by BrettG on Feb 16, 2012
Latest reply on Jun 8, 2012 by BrettG

Description:

It appears that with the latest Sigma Studio release (3.5), the flanger settings are not saved correctly.

This happens when the max delay is changed to something smaller than default value 500.

 

The problem can be demonstrated using these simple steps:

  • create a project and add a flanger effect.
  • change the delay from 10 to 1
  • change the max delay from 500 to 300
  • save the file
  • close the file.
  • when re-opening the file, the max delay field is now empty, and the delay field is 0. which results in the following error when I try to compile: "Index was out of range. Must be blahblah"

 

Please note that until closing/reopening the file, I can compile and the flanger effect works on my hardware.

 

SigmaStudio Version: 3.5

OS: Windows Vista Enterprise

Outcomes