AnsweredAssumed Answered

Build Error BF526 - blackfin-linux-dist-2011R1-RC3

Question asked by nick0mg on Feb 15, 2012
Latest reply on Feb 21, 2012 by nick0mg

I am attempting to build blackfin-linux-dist-2011R1-RC3 for BF526 EZBRD but it doesn't compile due to missing USB DMA functions. I have seen a couple of postings but no clear fix. Can anyone help?

 

Looks like its related to the default config

 

drivers/built-in.o: In function `musb_free':

/blackfin-linux-dist/linux-2.6.x/drivers/usb/musb/musb_core.c:1901: undefined reference to `dma_controller_destroy'

drivers/built-in.o: In function `musb_init_controller':

/blackfin-linux-dist/linux-2.6.x/drivers/usb/musb/musb_core.c:1982: undefined reference to `dma_controller_create'

make[1]: *** [.tmp_vmlinux1] Error 1

make[1]: Leaving directory `/blackfin-linux-dist/linux-2.6.x'

 

Thanks

Outcomes