AnsweredAssumed Answered

Problem with boot VDSP ldr-file

Question asked by to2nd on Feb 14, 2012
Latest reply on Feb 15, 2012 by sonic

Hi!

I'm compiling and flashing latest U-Boot release into Blutechnix's TCM-BF518 core module:

 

U-Boot 2011.09 (ADI-2012R1-pre) (Feb 02 2012 - 03:17:37)

 

CPU:   ADSP bf518-0.0 (Detected Rev: 0.1) (parallel flash boot)

Board: Bluetechnix TCM-BF518 board

       Support: http://www.bluetechnix.com/

                http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 100 MHz

RAM:   32 MiB

Flash: ERROR: too many flash sectors

8 MiB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin>

 

My project is LwIP application.

I'm creat ldr-file with VDSP 5.0 (update 10) with Loader options: Boot mode - Flash/Prom, Boot format - Binary,

and loading it in RAM:

 

bfin> tftp 8x.ldr

Using bfin_mac device

TFTP from server 192.168.65.45; our IP address is 192.168.66.45

Filename '8x.ldr'.

Load address: 0x1000000

Loading: ############

done

Bytes transferred = 176120 (2aff8 hex)

bfin>

I'm trying to boot it using "bootldr 0x1000000" command, but system crashed.

Where the find the bug?

Thanks.

Outcomes