AnsweredAssumed Answered

AD9889b  can't detecte  VIC  and no output video

Question asked by tanbo on Feb 9, 2012
Latest reply on Feb 10, 2012 by GuenterL

Dear all:

      input source is a single BT1120  YCbCr4:2:2  16bit  embedded sync  720p video input .    ad9889's pin6 clock rate is 74.25MHz ,pin4 frequency is 37.5KHZ, ad9889 can't detecte the source format.  The PLL indicates that it is locked; the TMDS drive is on,The difference signal was tested at a DC offset of 3V and have swings of about 500mV. The TMDS CK lines will run at the pixel clock rate (74.25)  ,   I think lots of reg is set right,but the 0x3e and 0x3f can,t detected ,  

What's wrong on it ? help me!  

 

The attach is hardware schematic:

here is the read back i2c value:

          0X00, 0X01, 0X02, 0X03, 0X04, 0X05, 0X06, 0X07, 0X08, 0X09, 0XA, 0XB, 0XC, 0XD, 0XE, 0XF

0X00, 0X0,   0X0,   0X0 ,  0X0,  0X0,   0X0 ,  0X0,   0X0,   0X0 ,  0X0,  0X41,0XE, 0X3C,0X18,0X1, 0X13

0X01, 0X25, 0X37, 0X0,    0X0,  0X0,  0X2,   0X31,  0X6A, 0XC,  0X52, 0X8, 0x0,  0x0,  0x0, 0X19,0XD7

0X02, 0X1C, 0X54, 0X8,   0x0,  0X1E, 0X89, 0X2,   0X92,  0x0 , 0x0,   0X8, 0x0,  0XE, 0X87,0X18,0XBD

0X03, 0X1B, 0X82, 0X80, 0X14, 0X5,   0X41, 0X59, 0XA,   0X0,  0X2d,  0X0, 0X1,  0X0, 0X0,  0X0,  0X0

0X04,  0X0,  0X10, 0X60, 0X7E, 0X78, 0X0,   0X0,   0X0,   0X0,  0X0,    0X0, 0X0,  0X0, 0X0,  0X0,  0X0

0x05,  0X0,  0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,  0X0,   0X0, 0X0,  0X0, 0X0,  0X0,  0X0

0x06,  0X0,  0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,  0X0,   0X0, 0X0,  0X0, 0X0,  0X0,  0X0

0x07,  0X0,  0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,  0X0,   0X0, 0X0,  0X0, 0X0,  0X0,  0X0

0x08,  0X0,  0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,   0X0,  0X0,   0X0, 0X0,  0X0, 0X0,  0X0,  0X0

0X09,  0X0,  0X0,   0X0,   0X0,   0XC0, 0X0,   0XE4, 0X0,   0XB,  0X2,   0X0, 0X18,0X5A,0X60,0X12,0X0

0XA,   0x0,  0x0,   0X80, 0X80,  0X8,   0X4,  0X0,    0X0,   0X0,  0X0,  0X0,  0X40,0X0,   0X0, 0X40,0X0

0XB,   0X5,  0XCD, 0X3F, 0XB9, 0X37, 0X7D, 0X20, 0XBC, 0X90,0X0,  0X0,  0X0,  0X0,  0X0,  0X0, 0X0

0XC,   0X0,  0X0,   0X0,   0X0,   0X0,   0X10,  0X4,   0X0,    0X2,  0X3, 0X0,   0X1,  0X2,  0X0, 0X0, 0X70

      

 

tanbo

Attachments

Outcomes