AnsweredAssumed Answered

UART Send without blocking

Question asked by russc243 on Feb 7, 2012
Latest reply on Feb 9, 2012 by Andreas

Hi,

I am using the UART on the BF561 to send data based on the code example in the DSP 5.0 install directory under the 561 EZ kit : UART-RS232 HyperTerminal (C). Most of the work is being done by the attached files.

 

In main, I can transmit like this: UART_puts("test 123") but it blocks. I need the 561 to continue processing data from an ADC so I don't want to wait for the blocking call to return.

 

Is there a simple example how to send with the UART without blocking? I don't want the complicaiton of using services.

Thanks

Russ

Attachments

Outcomes