AnsweredAssumed Answered

Selecting a Blackfin Eval board

Question asked by Kirby on Feb 8, 2012
Latest reply on Feb 10, 2012 by CraigG

I have a project that requires a camera input (type has not been determine), object tracking and overlaying. As well as dc motor control based object motion and a web server.  I have looked over the material on Analog website but am confused with the Blackfin Image Processing Toolbox and other software modules.  Some modules say that the ADZS-BF537-EZLITE-ND is not supported.  Is this just for demonstrations or all together? I selected this board because it was similar to the BF533 but included ethernet MAC.  Which embedded development board would you recommend, BF537, BF533, or BF561? Do I need the ADZS-USBLAN-EZEXT board or can I use one of the serial ports to connect to a third party serial to ethernet device.

 

Kirby

Outcomes