AnsweredAssumed Answered

ADAU1701 in self-boot mode with reduced power consumption ?

Question asked by BerndS on Feb 7, 2012
Latest reply on Feb 7, 2012 by BrettG

Hi all,

 

i need to know if it is possible to have the ADAU1701 (configured in self-bot mode) while powered down most of all chip sections (for reduced stand-by consumption) and observing an ADC for small signal input and start-up (function maybe called sleep mode with auto-power-on funktion) ?

 

Reason for this is the high current of ADAU1701 (1.8V and 3.3V) of about 100mA.  

 

thanks

 

Bernd

Outcomes