AnsweredAssumed Answered

Digital output voltage level on ADV7612

Question asked by Miroslav.cz on Feb 3, 2012
Latest reply on Feb 3, 2012 by GuenterL

Hello,

can I feed display with input voltage levels 1.8 - 2.5V directly (w/out level shifter) from ADV7612? In the HDMI rcv. datasheet is written - Output High Voltage VOH min 2.4 V - but there are no max. voltage or typical voltage datas.

 

Best regards

Miroslav Slovacek

Outcomes