AnsweredAssumed Answered

How to remove positive offset error for zero digital data in  AD5755BCPZ  ?

Question asked by VAV on Jan 25, 2012
Latest reply on Feb 14, 2014 by Edriano

 

 

 

Hi ,

 

The Digital Input data range  to any channel data-register of DAC IC AD5755BCPZ is ( 0x0000 to 0xFFFF )i.e ( 0 to 65535 in decimal )

 

Now if in case any positive offset output  ( Voltage or current ) is coming for zero digital input( 0x0000 ) then how can that be corrected i.e how can we   remove  positve offset error and get ( 0V or 0amp )  for zero digital input data ?

 

Is it that we have to use offset register ( as mentioned in the datasheet ) to remove any positive or negative offset error  ? if yes then please explain how  ?

 

Thanks & Regards !!

VAV

Outcomes