AnsweredAssumed Answered

Numeric format for State Variable (Q/F Input)?

Question asked by Dr.Ram on Jan 25, 2012
Latest reply on Jan 28, 2012 by Dr.Ram

Dear ADI Engineers:

 

I'm trying to use the State Variable (Q/F Input) in my ADAU1701 design but this modue is not documented at all in Sigma Studio 3.5. I'm having trouble figuring out what numeric format I should use for the F input. I'm pretty sure it cannot be 5.23 since that only allows values upto 15 or so; so is it 28.0 which would be pure decimal or is it something else?

 

I believe the Q-input is 5.23.

 

Thanks! - Ram

Outcomes