AnsweredAssumed Answered

Output compliance for AD911x?

Question asked by Reson8r on Jan 23, 2012
Latest reply on Feb 14, 2012 by Reson8r

Hi folks,

 

What is the output voltage compliance range for the AD9114-7 DACs with AVDD = 3.3V?  I see where the common mode voltage is -0.5 to +1.2 and the max full scale output current is 20 mA, but I don't see the DAC output voltage range limits.  Could I arrange the common mode voltage and output resistances such that the output voltage is 1.0 +/-0.5 V, for example?

 

Thanks,

Gerrit

Outcomes