AnsweredAssumed Answered

Relation of booting with internal RAM size

Question asked by srikanta on Jan 20, 2012
Latest reply on Jan 23, 2012 by AndyC

I have written a flash programmer driver for TS201 and it is working properly. Now Ihave one question and that is related with size of internal RAM of TS201.

In my board the flash size is 256M bits but the internal RAM size of TS201 is 24M bits. According to my knowledge, during booting process the code is loaded into the internal RAM of TS201 processor and it starts execution from 0x0 location.

Now if I write a code greater than 24M bits of TS201, how it can be stored in the internal RAM of the processor during booting process or how the code greater than 24M bits in the ROM/FLASH can be handled to perform the appropriate function.

 

 

Best Regards,

Srikanta

Outcomes