AnsweredAssumed Answered

mass_Storage_app_bf537 create a file on the virtual flash drive

Question asked by alexcalin on Jan 15, 2012
Latest reply on Jan 31, 2012 by CraigG

Hi,

I have the mass_storage_app_bf537,  I want to write a simple file on the virtual flash drive made of blackfin's SDRAM memory,  should I have in mind the FAT filesystem implementation before writing to its memory(allocation table,clusters and so on)?or should I simply write to bf's memory. I see from the .ldf file that the project defines 4(0-3) sdram memory banks, which one is used by the blackfin's virtual flash drive(if any)?

must further mention that I want to write a file..like say a simple text file to the virtual flash drive from within the mass_storage_app_bf537, I want it to be visible in the virtual flash drive as any other  plain file, when It is mounted.

So..please answer, very urgent!

Regards,

Alex

Outcomes