AnsweredAssumed Answered

AD8364 input power levels

Question asked by MandarN on Jan 15, 2012
Latest reply on Jan 17, 2012 by MandarN

In the datasheet  for AD8364 , there are different max and min input levels for different frequencies .

Are these experimental  limits used for calliberation of slope and intercept?

Can i use input power exceeding that given in the datasheet for the frequencies?

For example ,

for 2.14Ghz frequency, Max input level (Chan A/Chan B)   -  -2/-4

                                  Min input level (Chan A/ Chan B)   -  -57/-51

Can i use max - +5 and min -55?

Outcomes