AnsweredAssumed Answered

IS IT POSSIBLE TO INTERFACE A VIDEO TRANSMITTER WITH ANY OF THE BLACKFIN ADSP BFXX SERIES ??

Question asked by mahadeesh on Jan 13, 2012
Latest reply on Jan 23, 2012 by gyi

HI Friends,

 

WE are group of master students building small unmanned aerial vehicle(uav). We are planning to use  any of ADSP BF5XX series to perform certiain onboard image and video processing task in realtime on a flying platform. The input images and video for realtime processing is obtained from camera placed on the uav. Our intention is that, the captured input image and video has to be processed using ADSP BFXX( say applying some image processing algorithm on those image and video). Once the onboard processing is done, the processed video have to be transmitted to ground station which 500m away from the flying vehicle. Following are my doubts ??

 

1.  Is it feasible to implement entire mission using ADSP BF5XX series ??

2. If Yes, We are planning to use  2.4GHz 500mW audio/video TRANSMITTER. Is it possible to interface this transmitter with any of ADSP BF5XX    series?? I attached the video transmitter pic for ypur reference.

 

Thanks in advance for replying my query. Looking forward for your valuable suggestion.

Attachments

Outcomes