AnsweredAssumed Answered

does adv7510 capable of support 1900x1200 with reduced blanking

Question asked by hai on Jan 12, 2012
Latest reply on Jan 12, 2012 by cvaughn

adv7510 spec says it is capable of supporting an input data rate up to 165MHz, we would like to support WUXGA or CVR1960D (1920x1200 progressive, horizontal rate 74 kHz, vertical rate 60kHz, pixel rate 154MHz), since 154MHz is lower than 165Mhz, we think it should work, can anyone from ADI confirm? thanks!

Outcomes