AnsweredAssumed Answered

High Voltage High Frequency H-Bridge

Question asked by cmjosak on Jan 12, 2012
Latest reply on Jan 12, 2012 by bkennedy

I have been looking at the ADuM3220 and ADuM7234 and was wondering if you had any design suggestions or reference design for the following:  1) Need isolation, 2) Bridge voltage can be as high as 300V, and 3) Needs to drive a 20uH load at 1 MHz.  Also, can you tell me what the maximum switching frequency for the CN-0196 Circuit Evaluation Board is?  Can it be modified to run at higher voltages?

Outcomes