AnsweredAssumed Answered

Issue with generated header files in 3.5

Question asked by RyanJ on Jan 11, 2012
Latest reply on Jan 16, 2012 by RyanJ

I'm having an issue with inconsistent usage of the '_IC_1' suffix on definintions in my project header file in the released 3.5 (this is with windows 7, x64 compiling for an ADAU1446). Here are two examples:

 

#define NON_MODULO_RAM_SIZE 0
#define NON_MODULO_RAM_ADDR 24576
#define NON_MODULO_RAM_Data  0
...
SIGMA_WRITE_REGISTER_BLOCK( DEVICE_ADDR_IC_1, NON_MODULO_RAM_ADDRIC_1, NON_MODULO_RAM_SIZEIC_1, NON_MODULO_RAM_DataIC_1 );


#define PARAM_ADDR_IC_1 0

#define PARAM_SIZE_IC_1 148

...

SIGMA_WRITE_REGISTER_BLOCK( DEVICE_ADDR_IC_1, PARAM_ADDR, PARAM_SIZE, Param_Data_IC_1 );

 

 

If I revert back to 3.5.3 beta the problem goes away.

 

Thanks,

-- Ryan

Outcomes