AnsweredAssumed Answered

How to load and run a program from flash on BF516 target board using CrossCore Embedded Studio?

Question asked by youngpku on Aug 12, 2018
Latest reply on Aug 15, 2018 by youngpku

I am trying to load and run a program on BF 518F EZ board.

The instruction I found is for sharc, and I am following the CCES IDE option.

FAQ: How to load and run a program from flash on ADSP-SC5XX target board using CrossCore Embedded Studio? 

 

In the first step, creating ldr file, an initialization file is required.

I found a few files came with the CCES, including for the EZ board, and two versions for the 518 chip.

Which one should I use? What are the differences between them?

 

In the second step, a DPIA (device programmer interface application) file is required.

But I don't see it installed on my computer yet.

Can I download or build it?

 

Eventually, we are going to use our board with BF516.

Can I use the same initialization file and DPIA file for the ez board?

Or I need to create new ones?

Is there instruction for this?

Outcomes