AnsweredAssumed Answered

LTC3331 Solar Cell

Question asked by alanhawse on Aug 12, 2018
Latest reply on Aug 15, 2018 by alanhawse

The data sheet says that the maximum current is 50mA into AC1/AC2.

 

When I look at solar cells (from Digikey) it looks like the biggest solar cell that has a current <=50mA is 229mW

 

I guess my question is that it looks like there is a maximum IV depending with I fixed at 50mA... am I reading that right?

 

If you could find a solar cell that did 50mA @ 19V that which is about 1 Watt... but that solar cell doesnt seem to exist in the real world... and it looks like the biggest practical cell is around just a bit over 200mW.

Outcomes