AnsweredAssumed Answered

Confirmation of   status  meanning  for AD9375  2018_R1 version of NON-OS source

Question asked by okabe.y on Aug 7, 2018
Latest reply on Aug 7, 2018 by Vinod
Hi Team,
We are using 2018_R1 version of NON-OS source.
Status is displayed at line 520, line 527, and line 538 in headless.c.
(headless.c. is attached)
--------------------------- headless.c ---------------------------------
519 if (framerStatus! = 0x3E)
520 printf ("RxFramerStatus = 0x% x \ n", framerStatus);

526 if (obsFramerStatus! = 0x3E)
527 printf ("OrxFramerStatus = 0x% x \ n", obsFramerStatus);

537 if (deframerStatus! = 0x68)
538 printf ("DeframerStatus = 0x% x \ n", deframerStatus);
------------------------------------------------------------------------------------------
For example, if the "if" sentence of line 519 means that "RxFramerStatus is not 0x3E" is an error?
Regards,
Yoshihiro

Attachments

Outcomes