AnsweredAssumed Answered

The no OS mode with KC705 and AD9364

Question asked by tang71320 on Aug 6, 2018
Latest reply on Aug 13, 2018 by tang71320

Hello, I am a new guy for this part.  We want to use the no OS mode on our fmcomms4 board and KC705. 

I did step by step as the  AD9361 No-OS Software [Analog Devices Wiki]  show,

For the software  I use the sdk 2017.4

The hardware board is KC705 and Fmcomms4

The code source is from the hdl_2018_r1.

ALL the step is O.K until I run the configuration on SDK. I got this warning and feedback from the board.

The warning is "Given XMD transaction timeout value is invalid. Using default value of 60000 milli seconds"

The feedback is

"Failed to restore state
Failed to restore state
Failed to restore state
Failed to restore state
Failed to restore state
Failed to restore state
SAMPL CLK: 61440000 tuning: RX
0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
0:# # # # # # # # # # # # # # # #
1:# # # # # # # # # # # # # # # #
ad9361_dig_tune_delay: Tuning RX FAILED!
ad9361_init : AD936x initialization error
Done."

 

I Would like to know how to solve it ? AND which step may be the reason for this. 

BY the way, I did not get the screen like the link show

https://wiki.analog.com/_media/resources/eval/user-guides/ad-fmcomms2-ebz/software/fmcomms2_uart.png?cache= 

Attachments

Outcomes