AnsweredAssumed Answered

Replaceable DSP Code Sections in ADAU1452 or ADAU1466?

Question asked by edarring on Aug 6, 2018
Latest reply on Aug 15, 2018 by edarring

I'm wondering if it is possible to have sections of DSP code reserved to be replaceable.  Such sections would need to be identified such that the input and output connections are known.  The code inside the replaceable section would have a known maximum size, and can be replaced dynamically during runtime.  For a simple example:

 

 

Has anyone done this sort of thing?  Is it even possible?

 

Thanks!

Outcomes