AnsweredAssumed Answered

I am doing ADC characterization for 70 Mhz input and sampling at 240 MHz. I amusing ADC chips( AD9467).Some of the ADC parameters (such as SNR SNIAD,SFDR) are not met when digital board is fed with input more than 0dbm. Also Total Harmonic Distortion(THD)

Question asked by josh_g on Aug 3, 2018
Latest reply on Aug 3, 2018 by UmeshJ

I am using ADC chips( AD9467).Some of the ADC parameters (such as SNR SNIAD,SFDR) are not met when digital board is fed with input more. Also Total Harmonic Distortion(THD) values are not met for any input range.

For more details of my query please find the attachment. 

Outcomes